The History of Insulation Displacement Technology

The History of Insulation Displacement Technology
Written By: Hank Merkle
Abstract:
The need to physically connect pieces of metal together has been around for thousands of years. In the modern era of electronics, the physical connection requirement is compounded by the need for a low resistance electrical path. In both cases, the process of soldering has proven to be an excellent and time tested solution, with evidence dating back to 4,000 BC. Soldering two metal components together means that the joint is heated and a filler metal with a lower melting point than the constituent pieces is deposited to complete the connection.
DOWNLOAD TECHNICAL PAPER