LED Lighting Interconnects Solutions
Written By: Alex Guan
Abstract:
Solid-state lighting (SSL) solutions based on the light-emitting diode (LED) and its organic relative (OLED) have become the standard for luminaires across a wide variety of application sectors. SSL performance with respect to luminous output, power efficiency, lifetime, and reliability is unmatched. Many of the challenges endured by early adopters, such as cooling, manufacturability, and form factor limitations, have largely been solved. By the year 2035, it is projected that 85% of all lighting installations will be solid-state (“2019 Lighting R&D Opportunities”).
DOWNLOAD TECHNICAL PAPER
Solid-state lighting (SSL) solutions based on the light-emitting diode (LED) and its organic relative (OLED) have become the standard for luminaires across a wide variety of application sectors. SSL performance with respect to luminous output, power efficiency, lifetime, and reliability is unmatched. Many of the challenges endured by early adopters, such as cooling, manufacturability, and form factor limitations, have largely been solved. By the year 2035, it is projected that 85% of all lighting installations will be solid-state (“2019 Lighting R&D Opportunities”).