KYOCERA AVX has reached a final agreement with ROHM Semiconductor, which will transfer all of its tantalum and polymer capacitor manufacturing lines and relevant intellectual property to KYOCERA AVX effective August 5, 2022.
FOUNTAIN INN, S.C. (March 4, 2022) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, is set to acquire ROHM Semiconductor’s tantalum and polymer capacitor business assets. The two companies recently reached a final agreement, which states that ROHM Semiconductor (ROHM Co., Ltd.) will transfer its tantalum and polymer capacitor business assets — including all of its tantalum and polymer capacitor manufacturing lines and relevant intellectual property — to KYOCERA AVX. The transfer is scheduled to be executed on August 5, 2022, and ROHM will continue to produce tantalum and polymer capacitor products and supply them to KYOCERA AVX until all relevant production lines have been successfully transferred to the KYOCERA AVX manufacturing site. This will ensure a continuous supply for ROHM customers and immediately increase the already extensive selection of electrolytic capacitor solutions available to KYOCERA AVX customers.
“KYOCERA AVX is excited to announce the acquisition of ROHM Semiconductor’s tantalum and polymer capacitor business assets and to further expand our already extensive portfolio of electrolytic capacitor solutions,” said Johnny Sarvis, CEO of KYOCERA AVX. “KYOCERA AVX is the leading global supplier of tantalum capacitors, as well as the largest supplier of high-reliability manganese dioxide (MnO2) solid tantalum capacitors for medical, military, and aerospace applications. In addition, we have four global manufacturing plants to ensure we can deliver the flexibility and capacity required by these demanding markets.”
“Our polymer capacitors also offer significant advantages compared to others’ technologies, including high capacitance ratings in small, low-profile form factors, low ESR, stability over time, and a benign failure mode under recommended use conditions,” Sarvis continued. “In addition, they are environmentally friendly, lead-free, halogen-free, and RoHS-compliant and are ideal for use in commercial, industrial, automotive, and aerospace applications including smartphones, tablets, PCs, telecommunication systems, and solid-state drives.”
“KYOCERA AVX also has an open and progressive policy on ethical supply and is the first tantalum capacitor supplier to comply with OECD guidelines and legislation on conflict minerals, which are globally impactful achievements that we are incredibly proud of,” said Sarvis.
KYOCERA AVX’s portfolio of electrolytic capacitors includes an extensive selection of high-reliability, leaded, SMD standard tantalum MnO2, automotive-qualified, wet tantalum electrolytic, and high-temperature tantalum capacitors, and its portfolio of polymer capacitors includes an extensive selection of standard, high-voltage, small case size, SSD, high-reliability, and automotive-qualified polymer capacitors. Additionally, the recent launch of the aluminum electrolytic capacitor portfolio of standard wet, polymer, and hybrid capacitors allow customers more options for larger bulk capacitance solutions.
For more information about KYOCERA AVX, please visit https://www.kyocera-avx.com/, email inquiry@kyocera-avx.com, follow them on LinkedIn, Twitter, and Instagram, like them on Facebook, call 864-967-2150, or write to One AVX Boulevard, Fountain Inn, S.C. 29644.
About ROHM
Founded in 1958, ROHM provides LSI and discrete semiconductors characterized by outstanding quality and reliability for a broad range of markets, including automotive, industrial and consumer market via its global development and sales network. In the power and analog field, ROHM proposes the suitable solution for each application with power devices such as SiC, driver ICs to maximize their performance, and peripheral components such as transistors, diodes and resistors. Further information on ROHM can be found at https://www.rohm.com/