High-Temperature Capacitors Push Performance To 200°C And Beyond
Capacitors are among the most widely used passive components in electronics, so naturally they find their way into many applications in harsh operating environments. In certain applications such as those in oil logging, jet aircraft, nuclear power generation, and other industrial applications, these components are subject to extremely high temperatures, often somewhere in the range of 180°C to 300°C. how2power.com March 2022 Click to Read More