In addition to presenting an exhibitor seminar on the interchangeability of MLCCs & tantalum capacitors in high-capacitance applications, AVX is showcasing its expansive portfolio of tantalum, ceramic, power film, & supercapacitors ideal for use in multiple markets, including industrial, military, space, energy, consumer, telecom, medical, & more

FOUNTAIN INN, S.C. (March 11, 2019) – AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, is presenting and exhibiting at APEC 2019, which will take place in Anaheim, California, March 17-21, and provide attendees with five full days of technical sessions designed to address topics of both immediate and long-term interest to engineers in the applied power electronics industry.
AVX Technical Marketing Manager – Tantalum, Chris Reynolds, will deliver an APEC Exhibitor Seminar presentation that addresses industry-wide MLCC component shortages and potential solutions, “MLCC and Tantalum Electrolytic Capacitor Interchangeability in High-Capacitance Applications,” at 1:30pm on Tuesday, March 19, in Room 212AB.
Reynolds will also join several colleagues at Booth #832 in the APEC Exposition Hall March 18-20 to introduce attendees to the features and benefits of AVX’s vast portfolio of high-reliability power component solutions. Exhibition highlights include two new tantalum capacitor product releases: the TWA M39006 Series and F9H Series, several recently released product series, including tantalum capacitors, tantalum supercapacitors, and MLCCs, and a selection of popular and field-proven power component solutions.
New AVX Power Components on Exhibit at APEC 2019
AVX’s new TWA M39006 Series wet electrolytic tantalum capacitors are qualified to MIL-PRF-39006/33A and deliver high-reliability, high-CV performance in harsh-environment military, defense, avionics, and industrial applications, including satellites, DC/DC power supplies, power converters, bulk energy storage, and pule power circuits. Featuring a cylindrical, axial-leaded case with a hermetically sealed welded tantalum can and header assembly that ruggedly withstands environmental hazards including shock, vibration, and temperatures extending from -55°C to +125°C, as well as a unique cathode system that provides impressively high CV/cc and stable electrical parameters, the series offers high-reliability performance in voltage ratings spanning 25-75V, capacitance values spanning 470-1800µF, and T3 and T4 case sizes with M-level reliability (i.e., failure rates of 1% per 1,000 hours).
Additional AVX Power Component Solutions on Exhibit at APEC 2019
- AVX’s FHC1 and FHC2 Series power film capacitors, which smooth and filter current and voltage variations and prevent ripple currents from reaching power sources to protect high-power-density inverters in automotive, industrial, medical, mil/aero, consumer, communications, and alternative energy applications.
- AVX’s SCC Series supercapacitors and SCM Series supercapacitor modules, which combine very high capacitance with very low ESR and long-lifetime performance of 50,000+ cycles to achieve excellent pulse power-handling characteristics and can be used alone or in conjunction with primary or secondary batteries in the hold-up, energy harvesting, and pulse power circuits of various industrial, consumer, and telecom applications.
“APEC is the premier annual event for any and everyone involved in the power electronics industry,” said Reynolds. “We have been active participants in this conference for many years and are very much looking forward to this year’s conference, as there’s always a lot of great technical presentations and networking opportunities, and the expo gives us an excellent opportunity to introduce both current and potential customers to our newest power component solutions, which are always developed with the industry’s latest design demands in mind, if not especially designed to solve an existing application issue.”
Additional AVX exhibition highlights include a supercapacitor-powered demonstration, a wide range of sample kits showcasing the company’s various tantalum, ceramic, power film, and supercapacitor product portfolios, and several promotional giveaways to thank attendees for stopping by to chat with the engineering team.
To schedule an appointment with an AVX representative at APEC 2019, please contact Christina Sandidge, public relations specialist, BtB Marketing Communications, at christina.sandidge@btbmarketing.com or 919-872-8172.
For more information about AVX, please visit Booth #832 at APEC 2019, navigate to www.avx.com, email inquiry@kyocera-avx.com, follow them on LinkedIn and Twitter, like them on Facebook, call 864-967-2150, or write to One AVX Boulevard, Fountain Inn, SC 29644.