Antenna Simulation Models are now Available in Ansys HFSS 3D Electromagnetic Simulation Software

The latest release of the globally renowned software, Ansys 2023 R1, features direct links to simulation models for 13 of KYOCERA AVX’s most popular embedded antennas. These models are also available for Ansys versions 2019 R3 to 2022 R2, and a complete range of KYOCERA AVX embedded antenna models will soon be available for all of these versions.

FOUNTAIN INN, S.C. (March 28, 2023) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, is proud to announce that direct links to simulation models for its most popular embedded antennas are available in the latest release of the globally renowned Ansys HFSS 3D electromagnetic simulation software, Ansys 2023 R1.

Engineers use Ansys HFSS software to design high-frequency, high-speed electronics optimized for use in applications including communications systems, ADAS, satellites, and IoT devices. The latest release, Ansys 2023 R1, empowers users to run large jobs and overcome hardware capacity limitations with new high-performance computing and cloud capabilities, enhanced solver algorithms, and powerful graphical processing units. It also supports new collaborative, model-based systems engineering workflow capabilities and integrated more AI and machine learning capabilities to further improve engineering efficiency and accelerate innovation.

Ansys 2023 R1 features direct links to simulation models for 13 of the most popular KYOCERA AVX antennas, including embedded FR4 and ceramic GNSS, ISM, BLE, Wi-Fi, LPWA, 5G/LTE antennas widely employed in IoT, medical, and automotive applications. When users click on the 13 KYOCERA AVX antenna components featured in the Ansys 2023 R1 software, they will be transported to the KYOCERA AVX website to download the simulation files.

These 13 embedded antenna models are also available on the KYOCERA AVX website for Ansys HFSS versions 2019 R3 to 2022 R2. In addition, a complete range of KYOCERA AVX embedded antenna models designed for use with all of these versions will be available in Q2 2023.

“Many of our customers utilize Ansys HFSS software, and they used to have to contact us for compatible antenna simulation files. So, we’re very proud that our 13 most popular embedded antennas are featured in Ansys 2023 R1 and available for direct download on our website,” said Carmen Redondo, Director of Global Marketing Antennas, KYOCERA AVX. “We’re committed to providing our customers with a comprehensive suite of tools and resources engineered to make antenna integration as easy as possible and ensure optimal performance. So, we’re also proud to offer an increasing array of electromagnetic simulation model downloads compatible with Ansys versions 2023 R1 and 2019 R3 through 2022 R2 on our product pages.”

“We’re pleased to offer a selection of KYOCERA AVX’s embedded antennas in our new Ansys 2023 R1 software,” said Matt Commens, Senior Manager – Electronics Product Management, at Ansys. “The new products, technologies, and tools available in 2023 R1 enable engineering teams to simulate and rigorously examine products and systems under varying conditions, gain precise insights, and optimize designs at every stage of the product development process, regardless of application.”

For more information about KYOCERA AVX’s embedded antennas, antenna solutions portfolio, and antenna design tools, or Ansys HFSS 3D electromagnetic simulation software and the new 2023 R1 release, please click the embedded links. For all other inquires, please visit https://www.kyocera-avx.com/, email inquiry@kyocera-avx.com, follow them on LinkedIn, Twitter, and Instagram, like them on Facebook, call 864-967-2150, or write to One AVX Boulevard, Fountain Inn, S.C. 29644.