Validating the Long-Term Reliability of Self-Balancing Supercapacitors
It should come as no surprise that supercapacitors are becoming increasingly popular among board-level passive components. After all, these energy storage devices exhibit exceptional pulse-power handling capabilities as a result of their extremely high capacitance combined with very low equivalent series resistance (ESR). However, with this growing demand comes an increased need for supercapacitor reliability testing to accurately determine component failure rates, which play a crucial role in eliminating…
TechTimes.in
August 17, 2020
https://timestech.in/validating-the-long-term-reliability-of-self-balancing-supercapacitors/