FOUNTAIN INN, S.C. (November 7, 2016) – AVX Corporation, a leading manufacturer and supplier of passive components and interconnect solutions, has extended its J-CAP™ Series conductive polymer capacitors with conductive polymer electrodes, which already delivered the highest energy per volume (Joules/cc) of any SMT capacitor available on the market, with the addition of a new case size and several improved energy ratings. Now available in a large 7361-15 case with a low 1.5mm height profile, and capable of delivering up to an industry-leading 38.8mJ in low-profile SMD designs, J-CAP Series capacitors each feature a conductive polymer electrode that exhibits a benign failure mode under recommended use conditions, and undertab terminations that enable high both volumetric efficiency in small, low-profile case
Products – Whats New
FOUNTAIN INN, S.C. (November 2, 2016) – AVX Corporation, a leading manufacturer and supplier of passive components and interconnect solutions, has released a new series of supercapacitor modules. Comprised of series-connected cylindrical, electrochemical, double-layer supercapacitors, the new SCM Series supercapacitor modules are currently available in two voltage ratings (5V and 5.4V), and exhibit optimal pulse power handling characteristics, including: high capacitance values (0.47F – 7.5F ±20% tolerance), low ESR (4mΩ – 300mΩ at 1,000KHz), low leakage (2µA – 1,000µA), high energy density (1 to 5.6Wh/kg), and long lifetime performance (50,000+ cycles). Designed to provide reliable hold-up, energy harvesting, and pulse power solutions, SCM Series modules can be used alone or in conjunction with primary or secondary batteries to provide extended
FOUNTAIN INN, S.C. (October 31, 2016) – AVX Corporation, a leading manufacturer and supplier of passive components and interconnect solutions, has released a new series of cylindrical, electrochemical, double-layer supercapacitors. Rated for 2.7V and delivering high capacitance values (1F – 3,000F), low ESR (0.16mΩ – 200mΩ at 1,000KHz), low leakage (6µA – 5,800µA), high energy density (1.2 to 5.6Wh/kg), and long lifetime performance (50,000+ cycles), the new SCC Series supercapacitors exhibit excellent pulse power handling characteristics, and can be used alone or in conjunction with primary or secondary batteries to provide extended backup time, longer battery life, and instantaneous pulse power as needed. Available in a wide range of case sizes with diameters spanning 6.3mm to 60mm, case lengths spanning
FOUNTAIN INN, S.C. (October 26, 2016) – AVX Corporation, a leading manufacturer and supplier of passive components and interconnect solutions, has released a new series of low profile, low pass filters with best-in-class performance. Based on AVX’s patented and proven multilayer organic (MLO®) high density interconnect technology, the new LP Series MLO low pass filters utilize a combination of high dielectric constant and low-loss materials to enable the fabrication of multilayer, stacked passive devices, such as inductors and capacitors, with high volumetric efficiency, high Q, and exceptional electrical performance. Designed to support both a wide frequency range (0.4GHz – 6.5GHz) and several wireless standards, LP Series low pass filters feature an ultralow 0.55mm height profile, and exhibit excellent isolation, low
FOUNTAIN INN, S.C. (October 10, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, and the only authorized supplier of Kyocera Electronic Devices to the Americas and Europe, announces the 5236 Series µSIM memory card connectors from Kyocera Connector Products. Available in both single- and dual-card versions, both of which share a common PCB layout and feature 33% more signal pins than comparable connectors — eight for the single and 16 for the double — 5236 Series connectors feature a shell guide mechanism that prevents incorrect card insertion and unwanted ejection, enabling the secure operation of µSIM cards in mobile electronics, including smartphones and tablet PCs. Compact and low profile, with a minimal 0.7mm pitch, the
FOUNTAIN INN, S.C. (October 6, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has released a new 750MHz 0805 high performance, low pass integrated thin film (ITF) SMD filter that exhibits low insertion loss and extremely sharp roll-off in high frequency wireless applications spanning 746MHz – 756MHz, including: mobile communications systems, microcell and picocell base stations, satellite TV receivers, global positioning systems (GPS), vehicle location systems, and wireless large area networks (LANs). Based on thin film multilayer technology, the new 750MHz LP Series filter delivers excellent high frequency performance, and features an ultra miniature 0805 chip size with a rugged construction for reliable automatic assembly. “Wireless systems engineers rely on advanced electronic components, like our
FOUNTAIN INN, S.C. (September 22, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has added new 26VDC components to its proven, dual-function TransFeed™ and TransFeed Automotive Series varistors, extending the series’ superlative EMI/RFI filtering and bi-directional ESD protection capabilities to an even broader range of applications, including: automobiles, power supplies, computers, medical instruments, smartphones, multimedia add-on cards, barcode scanners, remote terminals, transceivers, and test equipment. TransFeed and Transfeed Automotive Series multilayer varistors (MLVs) are transient voltage suppression (TVS) devices that combine the most beneficial electrical characteristics of AVX’s robust TransGuard® TVS devices with those of its proven feedthru capacitors in a unique 0805 single-chip solution that responds to transient events faster than any other TVS
FOUNTAIN INN, S.C. (August 8, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, and the only authorized supplier of Kyocera Electronic Devices to the Americas and Europe, announces the 6411 Series PCI Express® M.2 connectors from Kyocera Connector Products®. Compatible with the new M.2 specification developed by the Peripheral Component Interconnect Special Interest Group (PCI-SIG), 6411 Series PCI Express connectors support multiple functions with high-speed signal integrity on a single card, effectively contributing to thinner and lighter notebook and mobile computers, including Ultrabook™ and tablet PCs. Designed to support high-speed, high-integrity PCIe Gen 3, USB 3.0, and SATA 3.0 signal transmissions for Wi-Fi, Bluetooth®, solid state drive (SSDs), global navigation satellite system (GNSS), near field
FOUNTAIN INN, S.C. (August 3, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has released a new 2.9GHz 0805 high performance, low pass integrated thin film (ITF) SMD filter that exhibits low insertion loss and extremely sharp roll-off in high frequency (1.7GHz – 2.9GHz) wireless applications, including: mobile communications systems, microcell and picocell base stations, satellite TV receivers, global positioning systems (GPS), vehicle location systems, and wireless large area networks (LANs). Based on thin film multilayer technology, the new 2.9GHz filter delivers excellent high frequency performance, and features an ultra miniature 0805 chip size with a rugged construction for reliable automatic assembly. “Wireless electronics engineers are constantly challenged to create smaller end products, and rely
FOUNTAIN INN, S.C. (July 25, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has added a locking plug to its low-profile 70-9159 Series single two-piece contacts for high current, coplanar PCB mating applications, which deliver the industry’s smallest profile capable of supporting a full 5A. The latest addition to AVX’s revolutionary, robust, and cost-effective portfolio of STRIPT™ insulator-less single contact solutions, the new 70-9159 Series locking plug contact features a positive latching mechanism that effectively replaces costly thermal adhesives, unreliable hand soldering, and large, light-blocking connectors in low-cost linear LED lighting, and a variety of other commercial and industrial coplanar and extended card applications. Based on AVX’s market-proven 9159 Series gold-plated beryllium-copper (BeCu) spring contact
FOUNTAIN INN, S.C. (July 18, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has renamed its revolutionary single contact technology. Introduced to the market in early 2011 as naked connector technology, AVX’s broad range of robust, insulator-less single contacts will now be sold as STRIPT™ connectors. STRIPT connectors are UL-certified single contacts that deliver the same performance as complete connector solutions without the additional space required by and assembly costs associated with a plastic insulator, effectively bridging the gap between hand soldering and one- and two-piece connector solutions. Based on unique board-to-board (BTB) and wire-to-board (WTB) single-contact designs pioneered by AVX, and constructed with premium base contact materials, STRIPT connectors enable engineers to meet stringent
FOUNTAIN INN, S.C. (May 31, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has released a new series of axial leaded, hermetically sealed wet electrolytic tantalum capacitors that achieve supercapacitor CV values in high temperature environments up to 125°C. Utilizing high CV tantalum powders and a well-established wet tantalum design, TWD High Temp Max Cap (HTMC) Series capacitors deliver exceptional electrical and mechanical stability, achieving extended operational lifetimes of up to 10,000 hours at 85°C, rated voltage. Combined with extremely high capacitance values spanning 25mF to 50mF and a wide operating temperature range spanning -55°C to +125°C, the extended endurance of the new TWD HTMC Series capacitors makes them ideal for use in DC hold-up
FOUNTAIN INN, S.C. (May 10, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has released a new series of low profile battery connectors especially designed to prevent end-user damage to the contacts in electronic devices with pluggable modules that vertically mate with a base unit. The new 9155-800 Series vertical-mate, 2mm-pitch battery connectors feature ultra robust and reliable gold-plated beryllium copper (BeCu) contacts that deliver excellent electrical and mechanical performance for more than 5,000 mating cycles, in addition to a unique contact geometry designed to deflect cleanly and easily when a module or mating connector is vertically pushed into position. The unique contact geometry of the 9155-800 Series allows for full vertical engagement in pluggable
FOUNTAIN INN, S.C. (May 5, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has released two new series of wire-to-wire (WTW) connectors that deliver considerable cost and space savings in a broad range of industrial electronics designs: the new 9286-200 Series reduced thru-wire connectors and 9286-250 reduced junction box connectors. These latest additions to AVX’s industry-proven 9286 family of poke-home discrete WTW connectors feature an active stainless steel spring contact with mechanical properties that allow it to provide maximum wire retention for 18 – 24AWG solid and stranded wire gauges. Capable of accommodating simple strip-and-poke-home wire insertion and twist-and-pull extraction, which is especially beneficial in field installations, these high-spring-force stainless steel contacts also effectively replace
AVX is the First to Achieve NASA’s S-311-P-838 Specification for Space-Level BME X7R MLCC Technology
FOUNTAIN INN, S.C. (May 4, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, is the first — and currently only — company to be recognized as a qualified supplier of space-level base metal electrode (BME) X7R dielectric multilayer ceramic capacitors (MLCCs) for use in aerospace designs and US military applications under the National Aeronautics and Space Administration’s (NASA’s) S-311-P-838 specification. This specification defines the requirements for high reliability, ceramic dielectric, multilayer, base metal electrode, fixed-value chip capacitors for high-reliability space applications, in addition to the processing verification and inspections required by assemblies used in flight. After several years of extensive testing and a meticulous, months-long review of the qualification data, AVX’s full range of space-level