Kyocera Begins Mass Production of Differential Clock Crystal OscillatorsDelivering Industry-Leading*1 30 fs Phase Jitter Enabling Low Noise, Low Power Solutions for AI Server Data Communication Kyocera Corporation (President: Hideo Tanimoto) today announced the launch and commencement of mass production in January 2026 of its “X Series” of differential clock crystal oscillators, achieving industry-leading low phase jitter of 30fs (femtoseconds) and low noise. Mass production commenced in January 2026. Differential clock crystal oscillators play an important role in enabling high-speed, large-capacity data communication in areas such as AI servers, offering enhanced noise resistance compared to standard clock crystal oscillators. Kyocera began mass production of the “X Series” in January this year with an initial monthly output of 200,000 units. In response
Learn More →Products – Whats New
KYOCERA AVX expanded its selection of 550/560 Series ultra-broadband capacitors to better satisfy surging demand for high-speed, high-bandwidth optical communication systems in a steadily growing range of cross-market applications. FOUNTAIN INN, S.C. (February 23, 2026) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, expanded its selection of 550/560 Series ultra-broadband capacitors to better satisfy surging cross-market demand for high-speed, high-bandwidth optical communication systems. The global optical communication systems market was valued at $36.87 billion in 2025 and is projected to be worth $74.21 billion by 2034 due, in large part, to the widespread proliferation of high-speed, high-bandwidth data transmission applications — ranging from online gaming and streaming
Learn More →Ultra-Compact, Ultra-Low Voltage: Kyocera Unveils the KC1210A Series Clock Oscillators Enabling Energy-Efficient Design for Next-Generation Smartphones and Wearables November 11, 2025 – Kyocera Corporation (President: Hideo Tanimoto; hereinafter “Kyocera”) announces the development of the KC1210A Series clock oscillators. These oscillators offer the world’s smallest size*1 and operate at an ultra-low voltage of 0.9V, which is approximately 50% lower than Kyocera’s previous conventional clock oscillator models. Sample shipments are now available, with full-scale mass production planned for the summer of 2026. KC1210A Series ■ Background of Development With the increasing functionality of smartphones and wearables, including AI, high-speed communication, large-scale data processing, and power consumption are also rising. This leads to faster battery depletion and more frequent charging. To address these
Learn More →Developed in collaboration with Iridium and qualified for use with Iridium Certus™ 9704 IoT modules, the new LDS cap antenna and evaluation board significantly outperform the ceramic patch antennas typically used in satellite IoT applications. FOUNTAIN INN, S.C. (November 4, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, launched a new LDS cap antenna and evaluation board optimized for Iridium® satellite IoT applications and designated as Iridium Qualified Antenna products for Iridium Certus 9704 modules. Developed to provide Iridium with an embedded antenna optimized for low Earth orbit (LEO) satellites used to provide seamless connectivity and data exchange for IoT devices anywhere in the world, the
Learn More →The new KGP Series commercial-grade stacked MLCCs are engineered to optimize the performance of high-frequency applications in the industrial, alternative energy, and downhole oil and gas industries and support the miniaturization and sustainability megatrends. FOUNTAIN INN, S.C. (October 13, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, released the new KGP Series commercial-grade stacked capacitors for high-frequency applications in the industrial and downhole oil and gas industries. The new commercial-grade KGP Series stacked multilayer ceramic capacitors (MLCCs) deliver higher capacitance values in the same mounting area as traditional capacitors to support the enduring miniaturization megatrend and are manufactured without lead or cadmium to support the thriving
Learn More →The new DSCC 25007 Mini BME Stacks deliver an unparalleled combination of high-reliability, high-CV performance, substantial space and weight savings, and standard 100% Group A testing to satisfy military and aerospace industry demands. FOUNTAIN INN, S.C. (September 8, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, released the new DSCC 25007 Mini BME Stacks — miniature, high-CV stacked X7R capacitors equipped with base metal electrodes (BME) and subjected to 100% Group A testing. Designed to satisfy the growing need for compact and lightweight high-CV SMT capacitors in high-reliability military, aerospace, and space applications subjected to extreme operating conditions and harsh environments, the new fully-tested and -traceable
Learn More →KYOCERA 5908 Series | Advancing High-Speed Connectivity Innovative Shielded Board-to-Board Connectors for Reliable EMI Protection Kyocera Corporation (President: Hideo Tanimoto) has developed the 0.4 mm pitch 5908 Series board-to-board connector, which is the first in its lineup to feature a fully shielded structure. Sales of this product, which enhances EMI characteristics by suppressing electromagnetic interference and supports high-speed transmission, began on Thursday, July 31. 2025 5908 Series Connector As communication and information processing technologies advance, devices such as smartphones and smartwatches require increasingly sophisticated connectors. Enhancing EMI characteristics during high-speed transmission has become a significant challenge for these applications. Kyocera addressed this challenge by introducing a fully shielded structure in the 0.4 mm pitch 5908 Series board-to-board connector, which effectively
Learn More →The new 9288-000 Series connectors enable quick, easy, and tool-free in-field termination; establish durable, reliable, high-integrity connections; and deliver excellent electrical and mechanical performance in lighting and industrial applications. FOUNTAIN INN, S.C. (August 7, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, released the new 9288-000 Series hermaphroditic wire-to-wire (WTW) and wire-to-board (WTB) connectors for lighting and industrial applications. These unique two-piece connectors facilitate WTW termination with two identical mating halves, which simplifies BOMs, and WTB termination with one those halves and an SMT version. Both halves of the new 9288-000 Series hermaphroditic connectors feature orange or white glass-filled PBT insulators equipped with plastic latches for
Learn More →The new 6780-000 Series IP20 T1 Industrial SPE connectors and cable assemblies offer significant space and weight savings and can also help reduce system complexity and costs and improve reliability and efficiency in applications including industrial automation, sensor, and actuator networks, smart grids, and traffic control and transportation systems. FOUNTAIN INN, S.C. (July 24, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, has introduced the new 6780-000 Series IP20 T1 Industrial Single-Pair Ethernet (SPE) connectors and cable assemblies. Designed to meet growing demand for smaller and faster Industrial Ethernet connectors capable of providing continuous communication and simplifying networks, the new 6780-000 Series T1 Industrial SPE connectors
Learn More →Designed to facilitate the continued evolution of high-frequency wireless systems in various market segments, the new DB0402 3dB 90° hybrid couplers provide repeatable high-frequency performance and continuous power handling in miniature, low-profile form factors compatible with automated assembly. FOUNTAIN INN, S.C. (July 1, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, released a new line of integrated thin film (ITF) hybrid couplers designed to facilitate the continued evolution of high-frequency wireless systems in industrial, automotive, telecommunications, and telemetry applications. Hybrid couplers are special four-port directional couplers that split input signals into two equal-amplitude 3dB outputs whose phases are shifted by 90°. Many also support performance monitoring
Learn More →The new 9155-900 Series 2.5mm-pitch vertical-mate battery connectors provide engineers in the industrial, automotive, datacom, household appliance, and consumer electronics markets with robust, reliable, and user-friendly power connectivity solutions. FOUNTAIN INN, S.C. (June 24, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, has further expanded its industry-leading selection of standard battery connectors with the introduction of the new 9155-900 Series 2.5mm-pitch vertical-mate battery connectors. The new 9155-900 Series 2.5mm-pitch vertical-mate battery connectors feature a unique contact geometry that deflects cleanly when a module, battery pack, mating connector, or PCB is vertically pushed into position, enabling full vertical engagement without the risk of contact damage. Traditional right-angle
Learn More →The new rugged, compact, and low-profile CP2816 Series integrated thin film (ITF) directional couplers satisfy cross-market demand for small, high-power couplers compatible with VHF and UHF bands. FOUNTAIN INN, S.C. (May 7, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, released the new CP2816 Series integrated thin film (ITF) high-directivity couplers for high-frequency wireless systems. Developed in response to customer requests for small, high-power couplers compatible with very- and ultra-high-frequency (VHF and UHF) bands, the new CP2816 Series ITF high-directivity couplers feature a rugged, compact, and low-profile 2816 (7x4mm) case and exhibit 20W continuous power handling, 50Ω impedance, and excellent high-frequency performance from 225–750MHz and -40°C
Learn More →KYOCERA AVX Unveils Worlds-First MLCC Delivering Industry-Highest 47μF Capacitance in 0402-inch Size
KYOCERA AVX Unveils World-First*1 Multilayer Ceramic Chip Capacitor (MLCC) Delivering Industry-Highest 47μF Capacitance in 0402-inch Size*2 KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, has successfully developed the world’s first*1 compact, high-capacity multilayer ceramic chip capacitor (MLCC) with an industry-leading capacitance value of 47µF in the 0402-inch size*2 (1.0mm x 0.5mm). Mass production scheduled to start in December 2025. The rapid evolution of artificial intelligence (AI) technology is driving a surge in demand for smartphones equipped with generative AI and AI servers. Additionally, as data processing technology becomes more advanced, the number of integrated components is increasing. Consequently, there is a growing need for ultra-compact components that allow
Learn More →The new BP1206 and BP2816 Series Thin-Film Band-Pass Filters deliver highly repeatable and reliable RF performance engineered for high-frequency wireless applications in the telecommunications, military, aerospace, medical, and consumer electronics industries. FOUNTAIN INN, S.C. (January 21, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, released two new series of compact, thin-film band-pass filters engineered to deliver excellent RF performance in a wide range of high-power applications with crowded PCBs. Designed to satisfy cross-market customer demand for small, high-power band-pass filters, the new BP1206 and BP2816 Series band-pass filters leverage the company’s proven, multilayer integrated thin-film (ITF) technology to deliver highly repeatable and reliable RF performance with
Learn More →The new 9140-000 Series two-piece STRIPT crimp contacts are compact, user-friendly, and reliable, optimized for space-constrained commercial, transportation, consumer, and industrial applications, and rated for up to 8A. FOUNTAIN INN, S.C. (January 14, 2025) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, released the new 9140-000 Series two-piece STRIPT® crimp contacts. Engineered to provide compact, reliable wire-to-board connections in commercial and transportation lighting, home appliance, consumer electronics, and industrial applications with space constraints ranging from densely populated boards to small form factors, the new 9140-000 Series features a UL-approved insulator-less design that utilizes the company’s industry-proven poke-home blade contact technology and measures just 4.6mm x 2.4mm x
Learn More →The new CR Series high-power chip resistor is non-magnetic, qualified to MIL-PRF-55342, and designed to deliver high-reliability performance in a variety of communications, instrumentation, test and measurement, military, and defense applications. FOUNTAIN INN, S.C. (December 12, 2024) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, expanded its selection of CR Series high-power chip resistors with the addition of the industry’s highest power 0603 resistor. CR Series high-power chip resistors are non-magnetic, RoHS compliant, qualified to MIL-PRF-55342, manufactured in ISO-9001 facilities, and proven to deliver high-reliability performance in a wide range of high-power and high-frequency applications. The new high-power 0603 resistors, which were developed to enable the miniaturization
Learn More →