Platform Structure Clock Oscillators Written By: Toshihiko Koyanagi Abstract: Numerous devices in people‘s lives today are becoming more sophisticated. As a result, the number of crystal devices installed is increasing. For example, with the evolution of autonomous driving, we are using crystal devices for many functions such as sensor systems to detect distance, camera systems to capture images, image processing systems to process captured images, and communication systems to communicate many of those digital data in and out of the vehicle at high speed. In addition, in the network market, the number of crystal devices is increasing along with the further increase in the speed of communication devices, as well as the increase in the frequency and precision. This paper
News / Events / Press
A growing number of applications, ranging from solar power converters all the way to miniature power supplies for highly complex processing cores, are starting to capitalize on the benefits of aluminum electrolytic capacitors. Aluminum electrolytics are also increasingly used to satisfy miniaturization demands in complex power tree applications like FPGAs powered by multiple voltages. And while it’s true that aluminum electrolytics also come with disadvantages, several of the more well-known ones are no longer true, and other perceived disadvantages can be reduced or eliminated by selecting newer components engineered to overcome some of the technology’s traditional shortcomings. Power Systems Design (PSD) December 22nd 2022
NEW | Multilayer Varistors Qualified to OPEN Alliance Standards for Automotive Ethernet Applications
As an OPEN Alliance member, KYOCERA AVX has extended its proven, high-performance, and ultralow-capacitance AntennaGuard range with the addition of two new MLVs that meet IEEE 1000BASE-T1 and 100BASE-T1 testing requirements, significantly outperform competing diode solutions, and deliver exceptional reliability in space-saving 0402 and 0603 packages. FOUNTAIN INN, S.C. (January 10, 2022) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, has extended its AntennaGuard range of proven, high-performance, and ultralow-capacitance products with two new 0402 multilayer varistors (MLVs) that meet IEEE 100BASE-T1 and 1000BASE-T1 testing requirements. The new ASPGuard® Series MLVs have small, ultralow-profile, surface-mount packages optimized for high-density designs and exhibit high current and energy handling
CES 2023 marks KYOCERA AVX’s first year of participation at this legendary industry event. Exhibit highlights include advanced antenna and RF component solutions for IoT, 5G, healthcare, consumer electronics, and satellite communications applications as well as advanced sensor and control solutions for electromobility applications. FOUNTAIN INN, S.C. (January 3, 2023) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, is exhibiting at CES 2023, which will take place Thursday, January 5, through Sunday, January 8, in Las Vegas. CES has earned a reputation as a proving ground for breakthrough technologies and global innovators and is widely recognized as one of the most influential tech events in the world.
SuperCapacitor Improvements on Small Generator Power Quality Written By: Ron Demcko | Ashley Stanziola | Daniel West Abstract: To expand portable electronics usage/reach/offering, the renewable power industry has taken an interest in the worldwide awareness of climate change and electronic waste, specifically how batteries affect the environment. One advancement is the emergence of modern low power hand crank generators, which roughly coincides with the accelerating interest in green energy used in portable electronics.
Predicting Metal Film Capacitor Lifetime Using Thermal Simulation Written By: Youssef Laamimat Abstract: In high-power applications like electric vehicles (EVs), customized metal film capacitors are often required to meet energy demands in a specific form factor. These capacitors exhibit a strong temperature dependence of their bulk capacitance over time, which directly limits their total service life. To maximize lifetime while minimizing space requirements, it is important to include accurate thermal simulation as part of the design process to ensure optimized and evenly distributed heat generation.
SuperCapacitors: A Reliable Backup Power Solution Written By: Johnson Jiang Abstract: Electric double-layer capacitors (EDLCs) are electrochemical capacitors called “SuperCapacitors,” or supercaps, due to their high energy density. Compared to traditional electrolytic capacitors, SuperCapacitors store electrical energy about two to three orders of magnitude higher and achieve several hundred thousand to millions of charge-discharge cycles. This advantage comes from the special construction of SuperCapacitors.
Electrostatic Protection Using Ceramic Capacitors Written By: Oliver Zimmermann | John McCarry Abstract: Any conductive interface between an electrical circuit and the outside world introduces the possibility of damage through electrostatic discharge (ESD). Accumulated static charge on a person, a cable, or any similar surface can readily dissipate its stored potential energy upon contact into sensitive components resulting in highly destructive currents. Ideally, varistors and TVS diodes only activate to protect the circuit when a high voltage is present and impart no parasitic effects during normal operation. For high-speed data lines, in particular, it is critical that the protection device introduce as little capacitance as possible (Electronic Design). TVS diodes and varistors are therefore specified not only by their voltage
High-Performance Battery Contacts for Mobile Electronics Written By: Ajay Saini Abstract: KYOCERA AVX offers the broadest standard battery connector line available on the market today. These robust connectors, available in horizontal and vertical options, are suited for battery pack integration and general board-to-board connection.
KYOCERA AVX’s new flagship facility in Nakhon Ratchasima, Thailand, features 1.2 million square feet of state-of-the-art design, manufacturing, testing, storage, and distribution space, meets FM Global standards, and features walkable ceilings, full electrical power supply redundancy, and column-free production areas. FOUNTAIN INN, S.C. (November 10, 2022) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, has announced the grand opening of its $300 million advanced manufacturing facility for ceramic and tantalum capacitors in Nakhon Ratchasima, Thailand. The new facility features 1.2 million square feet of state-of-the-art manufacturing and warehousing space. Deliberately designed as a safe and sustainable global facility for the production of ceramic and tantalum capacitors, the
The KYOCERA AVX team will showcase the company’s complete line of trusted and proven component solutions optimized for advanced automotive, industrial, and high-reliability applications, amongst others. FOUNTAIN INN, S.C. (November 8, 2022) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, is exhibiting at electronica 2022 in Munich, Germany, November 15–18. The KYOCERA AVX team will showcase the company’s complete line of trusted and proven component solutions at Booth 502 in Hall B4 (B4.502). Solutions on display will include advanced capacitors, antennas, interconnects, circuit protection and timing devices, sensors, controls, filters, fuses, diodes, resistors, couplers, and inductors optimized for employment in the automotive, IoT and IIoT, industrial, international
The new global MLCC part numbering system launching this November will maximize manufacturing synergies within KYOCERA AVX and the KYOCERA Electronics Components Group and make it easier for customers to search the entire brand portfolio. FOUNTAIN INN, S.C. (November 7, 2022) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, is introducing a new global MLCC part numbering system this November. The new global MLCC part numbering system will maximize manufacturing synergies within KYOCERA AVX and the KYOCERA Electronics Components Group, which combined their MLCC manufacturing and development resources in 2021 following the corporate reorganization and rebranding that elicited KYOCERA AVX. It will also facilitate the rapid expansion
Tantalum Capacitors in 5G Smartphone Applications Written By: Jason Liu Abstract: The global smartphone market has grown enormously over the past decade. In 2019, about 1.32 billion smartphones were shipped globally, of which 367 million units were shipped in China alone, accounting for 27.8% of the global total. With the ongoing investment into the construction of 5G networks, especially in China, 5G-enabled smartphones are set to become ubiquitous in the near future. 5G phones are projected to grow by 10% starting in 2020 compared to the previous year. Under favorable economic and regulatory conditions, there will be ample opportunities for both leading and emerging manufacturers to capture more market share. Additionally, there are several design houses for smartphones that design
Key Parameters for Designing Ceramic Capacitors in SMPS Circuits Written By: Kevin Cho Abstract: Capacitors are ubiquitous and indispensable components of electronic circuits used for a plethora of uses. For engineers looking to design multilayer ceramic capacitors (MLCCs) in switch-mode power supplies (SMPS) such as Buck and Boost converters, some essential parameters to be considered include the ripple current capability, ripple voltage, and power dissipation. Using the KYOCERA AVX SpiCalci10 model simulation tool for SMPS capacitors, this whitepaper will outline various MLCC characteristics, AC current capability, and other considerations for circuit design.
Advantages of Varistors and Their Applications in the Automotive Field Written By: George Zhang Abstract: Multilayer chip varistors (MLVs) are resistive elements comprising zinc oxide (Zn0) as the main component. In recent decades, they are being used for protection against surge voltage, noise, and transient voltages. Unlike conventional varistors, the maximum peak current and non-linear coefficients are large, and the resistance is very high below a threshold voltage, hardly allowing current to flow. However, when the voltage exceeds the threshold, the resistance drops abruptly and allows a large current to flow. Such properties make MLVs ideal as protective elements in a host of electrical and electronic applications, including automobiles
There are many places you could implement energy-harvesting (EH) sensors in factory automation and measurement applications. For example, remote or hard-to-access applications that currently rely on physical equipment inspections for status updates could be converted to a wireless sensor network, provided that there is enough energy nearby to capture and that the measurements are sufficient for making an informed decision. Control Design October 6th 2022