AVX will highlight the company’s state-of-the-art electronic components designed for real-world product applications in a nationally aired commercial on the Fox Business Network®, and in an upcoming production of the “Success” program FOUNTAIN INN, S.C. (October 18, 2018) – AVX Corporation, a leading manufacturer and supplier of advanced electronic components and interconnect, sensor, control, and antenna solutions, will be featured in a nationally aired commercial on the Fox Business Network® on Thursday, October 18, and Sunday, October 21, as well as in an upcoming production of “Success,” hosted by actor Rob Lowe. “Success” is an award-winning program that highlights innovative concepts and stories stemming from a variety of topics, including education, health, business, and more, through short-form and long-form documentary
News / Events / Press
Temperature Stability Assessment of GaN Power Amplifiers with Matching Tantalum Capacitors Written By: Ron Demcko | Mitch Weaver | Daniel West Abstract: Wide band gap GaN and SiC devices are expected to experience high levels of growth in applications ranging from power conversion to RF transistors and MMICs. End users recognize the advantages of GaN technology as an ability to operate under higher currents and voltages. RF GaN market is expected to grow at 22.9 % CAGR over 2017-2023, boosted by implementation of 5G networks. [1] During the past years, the wide band semiconductors have reported achievement of >1000 V BDV that opens new challenges for high power industrial applications such as electric traction systems in trams, trolley buses or
FOUNTAIN INN, S.C. (March 23, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has extended its proven F98 Series resin-molded, undertab termination style tantalum chip capacitors — known for providing miniature, low profile, and high CV solutions that reduce footprint, audio noise, and cost — with the addition of the industry’s smallest, highest CV 0603 tantalum capacitor rated at 100μF/6.3V. The new F98 Series 0603 capacitor delivers twice the capacitance of competitors’ 0603 tantalum capacitors, and halves the footprint of the 0805 component that had previously been the industry’s smallest tantalum capacitor with equivalent ratings. Free from the DC capacitance/voltage dependency that MLCCs experience and featuring SMD facedown, undertab terminations, which enable high volumetric efficiency,
FOUNTAIN INN, S.C. (March 21, 2015) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has released a new, high-voltage series of dry, medium-power film capacitors especially designed for DC filtering applications, such as the DC filtering of high frequency ripple currents and decoupling DC links in AC/AC and DC/AC motor drive inverters. Rated for 1.5kV to 3kV, the new FFLI Series capacitors are comprised of a unique combination of dry, metallized polypropylene film and a no-free-oil solution sealed in a cylindrical aluminum case filled with self-extinguishing polyurethane resin. This composition equips the FFLI Series with controlled self-healing technology, which prevents potential explosions resulting from avalanche effect, enables a benign failure mode consisting exclusively of capacitance losses,
FOUNTAIN INN, S.C. (March 17, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has extended its award-winning TCH Series high voltage, hermetically sealed polymer chip capacitors with the addition of a new 33µF/75V code. Packaged in robust, hermetically sealed ceramic cases filled with inert gas in order to eliminate the potential for materials and performance degradation resulting from exposure to high temperature, high humidity, and ambient atmosphere, TCH Series polymer chip capacitors — which were recently recognized with Electronics Weekly’s 2015 Passive and Electromechanical Product of the Year Elektra Award — are the world’s first effective polymer solution for mission-critical applications, including: automotive, avionics, aerospace, defense, pulse power, and power supplies. Manufactured and screened using
FOUNTAIN INN, S.C. (March 16, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, will be showcased in an upcoming production of Manufacturing Marvels, which is produced by Marvel Production Group, LLC, and will air on the Fox Business Network. AVX’s short, two-minute segment will focus on the company’s cutting-edge technology and real-world product applications — including: advanced automotive, satellite, telecommunications, consumer electronic, and medical device technology — and will air on Thursday, March 17, between 9:30 – 9:44 EDT. Produced by award-winning producers Bob and Jerry May, and narrated by CBS and ABC news veteran John Criswell, Manufacturing Marvels showcases American manufacturers and their products, processes, and customers in a promotional HD broadcast. “We are
FOUNTAIN INN, S.C. (March 16, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has added new high voltage components to its high reliability TWA Series COTS Plus axial leaded, wet electrolytic tantalum capacitors. Featuring a high capacitance cathode system that enables high CV levels in DSCC-compatible case sizes and new ratings as high as 4700µF/25V, 3000µF/50V, 2200µF/60V, 1000µF/75V, and 750µF/100V, TWA Series capacitors are ideal for use in high-reliability defense, avionics, radar, and power supply applications. “The new high CV ratings of the TWA Series COTS Plus wet electrolytic tantalum capacitors make them well suited for use in a wide variety of harsh environment, high reliability applications, and we’re still actively expanding the series,” said
FOUNTAIN INN, S.C. (March 14, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has extended its TWA-Y Series wet electrolytic tantalum capacitors with the addition of new, high CV 470µF/100V and 1,000µF/75V components. These components act as drop-in replacements for existing M39006-style wet tantalum capacitors in applications that may require operation at temperatures spanning 125°C to 200°C. TWA-Y Series wet tantalum capacitors are designed for continuous operation at 200°C (with applicable derating) and provide endurance ratings up to 2,000 hours. Featuring a unique cathode system that enables high CV performance in standard DSCC case sizes spanning T1–T4, TWA-Y Series capacitors deliver high reliability, high temperature, and long lifetime performance, and exhibit stable electrical parameters over
FOUNTAIN INN, S.C. (March 7, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has added several new capacitance and voltage ratings to its THH 230ºC Hermetic Series high temperature SMD tantalum capacitors, which, more than two years after their introduction, still feature the highest temperature ratings of any SMD tantalum capacitors available on the market. AVX has also improved the performance of the THH Series’ “I” case components, extending the maximum rated operating temperature from 215ºC to 230ºC. The series now features capacitance values spanning 6.8µF to 100µF, voltage ratings spanning 16V to 63V, and minimum lifetimes of 1,000 hours at 230ºC and 0.5VR and 10,000 hours at 200ºC and 0.5VR. Additionally, when compared with
FOUNTAIN INN, S.C. (March 4, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, will launch two new capacitor series, showcase its expansive portfolio of advanced passive solutions — including several new and significant series extensions, and contribute to the technical conference program at this year’s Applied Power Electronics Conference and Exposition (APEC 2016), which will take place March 20 – 24 in Long Beach, Calif. New AVX products slated for introduction at APEC 2016 include a series of next-generation, medical-grade tantalum capacitors that require much less voltage de-rating than any competitive offering and deliver both exceptionally low DCL values and extremely high reliability in a variety of medical implantable and life support devices, and a
FOUNTAIN INN, S.C. (February 22, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has extended the voltage ratings for its award-winning OxiCap® NOS Low ESR Series niobium oxide (NbO) capacitors to 8V at 85°C and 7V at 105°C to satisfy automotive applications requiring fail-safe SMD electrolytic capacitors, and has also added standard ESR ratings to satisfy more cost-conscious applications. Delivering exceptional reliability for SMD capacitors — 0.2% per 1,000 hours at rated voltage and 85°C, with just 20% recommended derating under load — the series is ideal for in-cabin automotive applications, such as: steering angle sensors, voltage regulators, DC-DC converters, electrochromic mirror systems, and automotive infotainment systems. Based on niobium oxide technology, which can withstand
FOUNTAIN INN, S.C. (February 9, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has introduced the robust new TCQ Series automotive conductive polymer chip capacitors. Qualified to the Automotive Electronics Council’s AEC-Q200 specification for passive components, the TCQ Series meets the AEC’s challenging 125°C lifetime stability test and humidity bias testing at 85°C and 85% relative humidity for up to 1,000 hours. “The AEC-Q200 lifetime stability and humidity bias tests are notoriously difficult for polymer capacitors to pass due to inherent material limitations. As such, we based our new TCQ Series automotive conductive polymer chip capacitors on our proven, high reliability TCR Series professional conductive polymer chip capacitors, making several critical improvements to the material,
FOUNTAIN INN, S.C. — The Board of Directors of AVX Corporation (NYSE: AVX) recently declared a dividend of $0.105 per common share for the quarter ended December 31, 2015. The dividend will be paid to shareholders of record on February 19, 2016 and will be disbursed on March 4, 2016. AVX, headquartered in Fountain Inn, South Carolina, is a leading manufacturer and supplier of a broad line of passive electronic components and related products. Please visit our website at: www.avx.com. Contact: AVX Corporation, Fountain Inn, SC Kurt Cummings, 864-967-9303 [email protected]
FOUNTAIN INN, S.C. (February 4, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has earned a third superlative for its F38 Series miniature, undertab, conductive polymer tantalum capacitors by significantly reducing the ESR of several ratings. The F38 Series, which already offered the smallest and highest CV polymer tantalum capacitors in the industry — 0603 capacitors with an ultralow profile of 0.9mm, and 6.3V/47μF ratings, now offers the lowest ESR small case size polymer capacitors available on the market as well. Made of conductive polymer materials and featuring SMD facedown terminals, which help enable low ESL and higher capacitance values in small case sizes, F38 Series capacitors exhibit high conductivity, low ESR, low ESL, and
FOUNTAIN INN, S.C. (January 27, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has been invited to present four technical presentations and chair a conference session at the 20th annual Components for Military & Space Electronics Conference & Exhibition (CMSE 2016), which will take place March 6–9, 2016 at the Sheraton Four Points Hotel in Los Angeles. Recognized as the most comprehensive conference dedicated to successful practices for the use of both military and COTS components in military and space systems, CMSE addresses topics including: electronic components, testing, reliability, and supply chain, and emphasizes new technology and design practices. CMSE 2016 will feature an intensive two-day-long, 17-tutorial training session about the impact of components on
FOUNTAIN INN, S.C. (January 5, 2016) – AVX Corporation, a leading manufacturer of passive components and interconnect solutions, has introduced the new T4C Series HRC4000 medical grade, solid tantalum microchip capacitors. Designed for use in the filtering, hold-up, timing, and pulsing circuits within implantable, non-life-support and non-implantable life support applications, the T4C Microchip Medical Series delivers the smallest medical tantalum capacitors available in the industry (0402 case sizes) with low DC leakage levels (0.01CV or 0.3μA), in addition to change control for consistent supply and high standard reliability better than 0.1% failures per 1,000 hours, which is 10 times better than standard commercial reliability. T4C Microchip Medical Series capacitors are manufactured and tested using AVX’s patented and extremely effective Q-Process