![](/images/Capacitor-Pi-Network-for-Impendance-Matching.jpg)
Capacitor Pi Network for Impedance Matching
Application Note 026
Abstract:
Designing matching networks is one of the key aspects of RF/Microwave design. A lossless network that matches an arbitrary load to real impedance has to have at least two reactive elements. However, two elements do not give control over the bandwidth and the degree of match simultaneously. Three-element matching networks, i.e. Pi- and Teenetworks, provide additional control of the frequency response.
DOWNLOAD ARTICLEDesigning matching networks is one of the key aspects of RF/Microwave design. A lossless network that matches an arbitrary load to real impedance has to have at least two reactive elements. However, two elements do not give control over the bandwidth and the degree of match simultaneously. Three-element matching networks, i.e. Pi- and Teenetworks, provide additional control of the frequency response.