The new AEC-Q200-qualifed VCAS Series MLVs feature soft terminations that provide up to 5mm of flexure over 3,000 temperature cycles extending up to 150°C with zero flex failures and stable electrical characteristics. The series also provides high current and energy handling capabilities, bidirectional overvoltage protection, and EMI/RFI attenuation in power and signal lines.
![](/en/wp-content/uploads/pr-images/kavx-mlv-with-flexiterm.png)
FOUNTAIN INN, S.C. (October 3, 2022) – KYOCERA AVX, a leading global manufacturer of advanced electronic components engineered to accelerate technological innovation and build a better future, has released the industry’s first automotive-qualified multilayer varistors (MLVs) equipped with the company’s patented FLEXITERM® soft termination technology, which has been widely employed on a number of automotive-qualified multilayer ceramic capacitors (MLCCs) for more than 15 years. Designed to satisfy automotive industry demands for more robust component solutions, the new VCAS Series MLVs with FLEXITERM® technology are engineered to reliably withstand severe flexing, vibration, and temperature cycling, enabling up to 5mm of mechanical board flexure over 3,000 temperature cycles extending up to 150°C with zero board flex failures, including internal cracks and depanelization, and no significant changes to electrical characteristics. Automotive-qualified MLVs with industry-standard terminations, on the other hand, generally support just 2mm of board flexure over 1,000 temperature cycles extending up to 125°C, which is often insufficient for preventing flex failures cause by the mechanical and thermal stresses incurred during assembly and operation.
As such, the new VCAS Series MLVs with FLEXITERM® soft termination technology provide increased reliability and outstanding mechanical and thermomechanical performance compared to competing solutions in automotive under-hood applications such as engine sensors with a direct connection to the battery rail, as well as in automotive audio circuits, aerospace, industrial, and downhole drilling applications, and IoT applications including smart watches, other wearables, and cleaning robots. In addition, these new MLVs exhibit high current and energy handling capabilities, super-fast response times, and multiple ESD strike capabilities, and provide high-reliability bidirectional overvoltage protection. They also provide EMI/RFI attenuation in their off state, which can reduce or even eliminate the need for additional EMC capacitors; exhibit lower insertion loss, lower leakage current, and unrivaled reliability compared to competing diode solutions; and are qualified to both the AEC-Q200 and VW 80808 specifications.
Currently available in four surface-mount cases sizes ranging from 0603 to 1210, the new VCAS Series MLVs are rated for five working voltages ranging from 5.6–30VDC, five clamping voltages extending from 18–67V, four energy transients spanning 0.1–1.5J, and operating temperatures as low as -55°C and as high as +150°C. They are also RoHS-compliant.
“We are very proud to introduce the new AEC-Q200-qualified VCAS Series multilayer varistors with FLEXITERM® technology to the market. This new product introduction will provide our automotive OEM customers with a compact, multifunctional component solution optimized for outstanding mechanical and thermomechanical robustness proven to reliably outperform competing MLV and diode solutions in harsh-environment signal and power line applications subject to vibration, variable temperatures, and flexure stress,” said John Gallipeau, Senior Field Applications Engineer, KYOCERA AVX. “As the demand for more electronic content in today’s vehicles continues to grow, so does the demand for extremely rugged and reliable electronic components qualified for use in these challenging applications. As such, the new VCAS Series MLVs are just the first to feature our patented and field proven FLEXITERM® soft termination technology. Soon, all of our TransGuard® and TransGuard Automotive MLVs will also be available with FLEXITERM® technology.”
When subjected to the rigorous AEC-Q200 board bend and temperature cycling testing procedures, the new VCAS Series MLVs with FLEXITERM® technology were proven to withstand up to 5mm of flexure (versus 2mm for MLVs with industry-standard terminations) over 3,000 temperature cycles extending up to 150°C with zero board flex failures and no significant changes to their electrical characteristics, which well exceeds the 1,000 cycles at up to 125°C AEC-Q200 testing requirement. This proven performance makes the series ideal for use in the signal and power lines of automotive, aerospace, and IoT applications subject to hazards including significant temperature variations, vibration, wave soldering, forced cooling, improper handling, the insertion and removal of PCBs from connectors, and high-density board configurations, all of which can result in board expansion, contraction, flexure, and cracking, and the depanelization of components mounted near the edges of the PCB, near flex zones, and near large, heavy components.
VCAS Series MLVs with FLEXITERM® technology are packaged on 7” reels for compatibility with automated processing equipment, and lead-time for the series is currently 10 weeks.
For more information about KYOCERA AVX’s new VCAS Series multilayer varistors with FLEXITERM® technology, please visit click product button below. To order, please visit Digi-Key Electronics and Mouser Electronics. For all other inquires, please visit https://www.kyocera-avx.com/, email inquiry@kyocera-avx.com, follow them on LinkedIn, Twitter, and Instagram, like them on Facebook, call 864-967-2150, or write to One AVX Boulevard, Fountain Inn, S.C. 29644.